網站維護通知 6月22 - 24日
本網站將於6月22日(週六)淩晨03:00 - 6月24日(週一)早上05:00 期間進行系統維護,維護期間您將無法訪問。如因此對您造成不便,我們深表歉意!
本網站將於6月22日(週六)淩晨03:00 - 6月24日(週一)早上05:00 期間進行系統維護,維護期間您將無法訪問。如因此對您造成不便,我們深表歉意!
Oscilloscope probes are a type of device commonly used by electrical engineers that can connect a signal source to an oscilloscope. The probe is a single input device that can divert the electrical signal to the scope. Oscilloscope probes can be used in various applications and can range from a simple wire like a passive probe to a more complex device.
An oscilloscope is considered to be the most used instrument for electrical engineers who need to measure electrical characteristics of electronic devices but you also need at least one probe.
The best approach, for matching a probe with a scope, is to first choose a probe whose capacitance is within the range of your scope and then fine-tune the probe's capacitance by adjusting its compensation network using the probe's trimmer capacitor.
The 1X probes are suitable for many low frequency applications. They typically offer the same input impedance of the oscilloscope which is normally 1 M Ohm. The most common type of probe with a built in attenuator gives an attenuation of ten, and it is known as a 10X oscilloscope probe.
Passive probes are the most commonly used probes for taking measurements. They are easy to use, relatively inexpensive, and fairly rugged. Available in the following configurations:
Attenuation probes serve to multiply the voltage measurement range of the oscilloscope by using an internal resistor that, when used in conjunction with the input resistance of the scope, creates a voltage divider. Useful for the following reasons:
Active probes contain active components, such as FETs or amplifiers. Commonly used for taking high-speed measurements (>500 MHz) or on high-impedance circuits. One limitation is their limited voltage range.
Differential probes are popular for measuring high-frequency signals or signals of very low amplitude.
A current probe measures the electrical current flowing through a conductor.