最近搜索

    Bulkhead Lights

    Bulkhead lights, also known as bulkhead lights or deck lights, illuminate the interior of boats, RVs, and other vehicles. They are typically mounted inside a vehicle's cabin or compartments and are often used to decorate storage areas and utility rooms. Bulkhead lights can also provide general illumination in places where it may be challenging to install conventional lighting fixtures, such as under stairwells or along hallways.

    Bulkhead Ceiling Light

    Bulkhead ceiling lights are a great way to enhance the look of your home, office, or boat. They're available in a wide range of styles, shapes, and sizes, so you can find one that will suit just about any space. Bulkhead ceiling lights come in different materials and finishes, so you can choose the one that best suits your needs.

    Bulkhead ceiling lights are designed to be installed on the bulkhead wall or ceiling. The bulkhead is an area of wall between two vessel sections, such as an engine room or cabin. Bulkheads have electrical circuits and usually contain watertight doors to protect from flooding. In many boats, bulkheads are also used for storage and other purposes.

    The bulkhead is usually painted black, but some boats have them painted white or other colors to match up with their decorating scheme. The bulkhead light itself should be located near the center of the bulkhead, so it shines down on the deck below it and doesn't shine directly into anyone's eyes while they're working below the deck.

    LED Bulkhead

    LED bulkhead lights are one of the most popular options for marine lighting. This type of light has a lot of benefits over conventional incandescent bulbs. It offers brighter light and consumes less power than other types of bulbs. LEDs also last longer than incandescent bulbs, so you do not have to replace them often. These lights come in various colors, so you can select one that perfectly matches your boat’s interior design.

    Industrial Bulkhead Lights

    The industrial bulkhead light is an excellent choice for those requiring lighting in areas with no power source. The bulkhead light is designed to be mounted directly to the wall or ceiling, and it can be used in many different areas, such as commercial buildings, warehouses, and factories. These lights are also great for outdoor use, especially if you need to illuminate large areas such as parking lots or loading docks.

    The best part about these lights is that they are waterproof and corrosion-resistant, which means they can withstand harsh weather conditions and high humidity levels without any problems whatsoever. These lights come with various mounting options, so they can be installed almost anywhere you want them installed!

    篩選條件
    排序方式
    1
    0
    每頁
    1
    0
    每頁